This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L11: ADS127L11前端放大器选型问题

Part Number: ADS127L11
Other Parts Discussed in Thread: THS4551, OPA2189

1、待测信号是全桥信号,全桥供电5V,全桥输出信号频率最大=1khz。最大峰峰值Vo=Vp-Vn=30mV

2、我发现在任何滤波模式下,high-speed-mode的有效位数基本上都比low-speed-mode要高。

3、前期使用测试过程中会使用high-speed-mode和low-speed-mode,使用到的数据速率 <= 400KSPS.

4、增益=50;

5、因为待测信号频率比较小,所以adc前端的混叠滤波器-3dB带宽只要 > 1khz就行了,尽量大一些,我估摸着-3dB太小的话滤波器阶数会太多;

6、手册9.2案列是考虑到使用条件比较苛刻的时候,才把-3dB调到500Khz,并要求在Fmod=12.8Mhz处衰减90dB。我这次的测试要用到high和low两种速度模式,所以应该要求在低速模式的调制频率下Fmod=1.6Mhz处,尽可能的衰减,比如也衰减到90dB。

7、开启ADC内部的precharge-buff功能,我不打算用高带宽的全差分放大器,比如THS4551,因为他的输入失调电压漂移太大了,比ADC本身的都大。所以我打算用OPA2189,它的各方面参数都很好,只是带宽太小了,才14Mhz。我初步的设想有2钟方法。

     a、OPA2189组成仪表放大器,然后再配合几阶混叠滤波器,尽量提高在1.6Mhz处衰减量。

     b、如果“a”不行,就把OPA2189组成Multiple FeedBcak(MFB)拓扑结构的滤波器,再配合几阶混叠滤波器搞一搞,看看仿真效果怎么样。

我困惑的地方是,有增益50倍,放大器带宽小,ADC采样率会使用高速模式下的400KSPS,选的这个OPA2189能合适吗