This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1211: ADS1211有效数据位数,数据输出波动大

Part Number: ADS1211
Other Parts Discussed in Thread: REF5050,

ADS1211使用内部电源参考,芯片模拟电源和数字电源分开,均采用REF5050,采样频率100HZ时,输出数值有1700的波动,是否说明当前芯片有效位数仅有13位左右?如此,需要提高芯片有效位数,有哪些好的方法?希望得到帮助,谢谢!

  • 您好,

    提高ADC的有效位数,除了降低参考电压和供电电源的纹波外,还与ADC的配置有关,相关参数有Data rate、Clock 频率、TURBO MODE RATE、PGA值,具体见数据表第7页曲线图,如下截图

    或者如下表格截图:

    总的来说,降低Data rate、降低PGA、增加采样频率可以提高有效分辨率。

  • 感谢您的回复,我当前晶振10MHZ,采样速率100HZ,PGA:1,加速因子:16,手册上为22.5位有效位数,实际我测试有1700的波动范围,请问这个正常吗?

  • 实际我测试有1700的波动范围

    您的意思是后11位都是波动的?这不正常,误差太大了;

    您输入的信号是什么?输入信号范围是多少?看下是否满足ADC输入信号范围;

    芯片模拟电源和数字电源分开,均采用REF5050,

    ADC工作时,用示波器实测下AVDD电压存在波动吗?

    另外,是否验证了寄存器的读写功能,写入已知数据后是否可以正确读出来?