Other Parts Discussed in Thread: ADC3683


In the ADC3683EVM diagram, as shown by the left figure, there is an LPF(0~30 MHz) before the ADC3683. However, the datasheet (the right figure) of ADC3683 shows that the 3-dB bandwidth of ADC3683 is 900MHz. Does the LPF affect the ADC's performance if a signal with frequency larger than 30 MHz (such as 500 MHz) is sent to the AD3683EVM?