Part Number: ADS1299
进行内部方波测试时,配置config1---- 0x96 ,config2---- 0xd0, config3---- 0xec,得到内部测试信号测量值不对,其值为-2.375mv到+1.475mv,不是标准的方波±1.875mv,并且内部噪声测试时,其值为-590uv左右。
测得vrefp为2.393v,vrefn为-2.517v,测得spi时序是正常的,请问我下一步该怎么去检查,才能解决这个问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不使用的模拟输入应连AVDD;

不使用的GPIO应经电阻接DGND;

数字地和模拟地分开的话,31脚 RESV1应接DGND;DGND相应管脚应接DGND;

START pin不可以悬空:

并且测得vcap1 -0.615v vcap2 -0.021v vcap3 4.336v vcap4 -1.827v 。vcap1达不到1.1v
检测下是否符合数据表 11.1 Power-Up Sequencing的上电顺序;
另外,根据下面链接检查下芯片是否是正常的
是的,使用内部参考的话,这里vrefp-vrefn也要是4.5v,±0.2%的精度;