Other Parts Discussed in Thread: TVP7002
最近在调试TVP7002(VGA接口)芯片,发现7002裸板在室温下正常工作时的芯片温度为60度,十分烫手,查了一下电源好像也没什么异常,希望哪位有用个的高手指点一下调试方向。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TVP7002
最近在调试TVP7002(VGA接口)芯片,发现7002裸板在室温下正常工作时的芯片温度为60度,十分烫手,查了一下电源好像也没什么异常,希望哪位有用个的高手指点一下调试方向。
Hi
建议你先确认一下你的layout, 按照datasheet “Junction-to-ambient thermal resistance, still air ,Thermal pad soldered to 4-layer High-K PCB), 热阻是17.28℃/W, 按照参数表:PTOT Total power dissipation, normal mode 1403mW, 芯片的温度将是25+17.28*1.403=49.24℃
如果你layout是按照这种情况, 你需要检查芯片PowerPAD的焊接以及散热设计。
如果你增加Junction-to-case的设计,这种情况下热阻比较小,就不会出现上述温度过高的情况。
已经查明是7002的PowerPAD的焊接问题(没有完全接触),对芯片做加热在使用镊子将芯片往下按处理后工作正常(温度恢复至43℃左右);
芯片实际PowerPAD尺寸是6.2*6.2mm,我们的封装尺寸采用的6.5*6.5mm的PowerPAD设计的,增加PowerPAD的封装尺寸是否可以上述问题,或者有其他更好的方法?
增加PowerPAD的封装尺寸是否可以避免上述问题,或者有其他更好的方法?
显然你的PowerPAD面积过小,如果想更好的散热,可以将PowerPAD两面都覆铜,并且过孔连通。
对热设计感兴趣,推荐阅读
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slma002
Hi
增加powerpad的面积,如打孔到其他板面GND层,帮助散热,是可以芯片降温。如果你的要求是50℃以下(25℃环境下),如之前的计算,完全是没有问题的。
如果想更好的降温,采用可以Junction-to-case的设计,这种情况下热阻比较小,温度更加低。