Other Parts Discussed in Thread: ADS54J60EVM, , ADS54J69

要实现DC耦合输入的方式,对电路连接的修改是否是:断开R7,用o ohm电阻连接R4、C3即可?以下附件是评估板的原理图以及实物图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

要实现DC耦合输入的方式,对电路连接的修改是否是:断开R7,用o ohm电阻连接R4、C3即可?以下附件是评估板的原理图以及实物图:
您好,
上图中默认是单端变压器耦合输入,变压器耦合输入属于AC耦合输入;
如果采用DC耦合输入的话,需要将通道 A 上的 C6,C7和 R7卸下,然后安装 R3,R4,C1和 C3, 所有电阻器和电容器值均为0Ω电阻;
另外请注意,输入信号(INP、INM)必须满足 ADC 所需的输入共模电压VCM=2V;
如果您的输入信号是单端信号的话,恐怕需要通过全差分运放将单端信号转换成差分信号,因为ADS54J69的每个输入管脚INP和INM,都需要共模电压在2V