小弟想知道官方手册中的LM8272组成的参考电压电路最多能同时驱动多少片ADC08200,小弟要用到4片AD,求高手指点,非常感谢~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照datasheet : http://www.ti.com.cn/cn/lit/ds/symlink/adc08200.pdf 第十六页的电路,VRT − VRB电压是1.6V, Reference Ladder Resistance典型值是160欧姆,最小是120欧姆,最大电流可以达到13.3mA. 4片的电流53mA
按照运放:http://www.ti.com.cn/cn/lit/ds/symlink/lm8272.pdf 规格 Output current (1V from rails) ±65mA , 但是按照上述电路,LM8272 输出到VRB的电压是0.3V, 不在1V from rails的范围内,它的sink是达不到65mA, 会比较小,见datasheet 第九页第四个图.
如上应该是带不动4片AD的, 至多2片。 建议你按照LM8272 搭一下,看按照这个电路最大能有多大的负载能力?(LM8272 sink电流的曲线图数据不明显),或者你在运放的论坛上讨论一下。
Hi
关于运放的选型建议你到放大器对应的论坛进行讨论: http://www.deyisupport.com/question_answer/analog/amplifiers/f/52.aspx
找了一下大电流输出的运放,在较低电压输出的sink电流都不大,建议找运放的工程师推荐一下。