This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用ADS1198-FE遇到的问题,急!



使用ADS1198-FE,下载了软件按照说明进行了调试,但出现了两个问题:

1、工频干扰特别大,淹没了有用信号。后来我直接将通道2与信号发生器相接看波形,依旧有非常大的干扰,几乎看不到波形。

2、在测试MVDD时出现问题,DVDD/2应该是3.3V/2=1.65V左右,但显示一直为0.8V左右,我已经把DVDD调成3.3V了,用万用表测量板上的电压也是3.3V,另外把AVDD设成3V,AVSS设成-2.5V,通道显示的值一直为2.4V

 

主要是第一个问题啦,我想用它来测试肌电信号的,干扰特别大(已经接了右腿驱动),没想到用信号发生器输入波形都看不到,求解