This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5686: DAC5686输出的P,N端区分

Part Number: DAC5686


Hi,

有两个问题:

1. IOUTA1,IOUTA2和IOUTB1,IOUTB2,这两对差分哪个是P端?哪个是N端?在规格书上看不出来。

但是从参考电路上去看IOUTA1,IOUTB1是N端,IOUTA2,IOUTB2是P端。这个理解对吗?

2. 哪对是接I信号?哪对是接Q信号?

  • 参考电路上去看IOUTA1,IOUTB1是N端,IOUTA2,IOUTB2是P端。这个理解对吗

    您好,您的理解是对的,或者数据手册Analog Current Outputs这部分也提到了,IOUT1是positive端,IOUT2是Negative端。

    哪对是接I信号?哪对是接Q信号?

    如果使用dual bus mode,DA可以接I,DB接Q,但是如果使用Interleave Bus Mode,I和Q都接在DA channel上。