This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8318: SDO波形异常

Part Number: ADS8318


TI专家,您们好,

     客户在使用ADS8318过程中,遇到SDO波形异常情况。

     读取数据的时候正常,不读取数据的时候,出现一个1.2V到2V的斜坡。请问是什么情况?谢谢。

  • 您好,

    我想可能与SDO信号线上接下拉电阻R9214到地有关,因为ADS8318的SDO在不输出数据时进入三态状态,如果在SDO上接下拉,可能会出现上述情况,您将R9214去掉,看是否解决问题?