你好,
我们在进行开发时,发现在输出5MHz正弦信号时,输出功率大概为2.6dBm,输出50MHz正弦信号时,功率大概为0dBm,
请问问题可能出现在哪里呢?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下面链接是我咨询美国工程师的帖子,我已将您的信息反馈给他,您在下面链接看到答复后,也可以直接跟进帖子,以节省我在中间转话的时间:
Attached are power measurements with tones at 5MHz, 50MHz and 100MHz with the DAC sampling at 625MHz. This is using the TI DAC38JxxEVM.
美国工程师给出了使用DAC38JxxEVM 设置DAC采样频率为625MHz时的功率测量,见附件,它们分别在单音信号为5MHz,50MHz和100MHz时测得的:
波形文件见附件。 每个文件有两列数据。 第一列发送到DAC A,第二列发送到DAC B ;