This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADCS7476: ADCS7476 digital input is independent with AVDD

Part Number: ADCS7476


in datasheet discription, adcs7476 digital input voltage is independent with avdd,

is it mean that (digital input = 5V && AVDD = 3V ) or ( digital input = 3V && AVDD = 5V) allowed??

looking forward to your reply, thank you! 

  • 您好,

    这两种情况都是可以的,因为数字输入引脚限制电压与电源电压VDD无关,数字信号输入电压最大可以到6.5V,而可以识别为高电平的电压是2.4V;

    另外,请注意尽管数字输入可以达6.5 V,但数字输出只能驱动VDD的电压输出。