Other Parts Discussed in Thread: ADC08060
现在按官方的电路调试ADC08060,输入时钟,没有数据输出,请问应该如何去调试呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
也先确认一下你的电路,见datasheet: http://www.ti.com.cn/cn/lit/ds/symlink/adc08060.pdf 第16~18页。
主要是需要一个较高的CLK频率,例如 fCLK = 60 MHz at 50% duty cycle(需要高出20MHz), 你需要确认一下。
datasheet不是说20M~60M吗?我现在试了,用20M的时钟了,没有什么输出来。是不是20M的时钟满足不了这个芯片的需求。
Hi
你可以试一下更高的频率,但是20MHz是没有问题的。
模拟输入电压的范围是Vrb~Vrt, 确认一下?
另外确认一下芯片, 可以找e络盟(TI的小批量代理商): http://www.ti.com.cn/general/cn/docs/gencontent.tsp?contentId=24957
我用20M的时钟,试了输入电压是 VRB ,VRT了,输出结果基本一样,理论上,这两个的结果是很不一样的,我的电源供电是3.3V,应该没有什么问题吧?
Hi
不要超过电压Va=3.3V就不会导致芯片烧坏。但是有效的转换电压范围是Vrb~Vrt.
另外电路上注意一下DRDV是有bypass电容的。
如之前谈到,确认一下芯片的质量。