我在使用ads1248串联3路PT100进行测温时,电路板在手动上下电(冷启动)或者不下电复位主控MCU时,有几率性出现温度测试结果异常现象,温度比实际值相差较大,例如测室温在26℃左右,但测温电路测试结果达30甚至40℃。测温电路及其供电电路图如下图所示:

PT100传感器及线路连接已确保没问题,PT100阻值随温度变化也正常,参比电阻精度0.01%。
随后用示波器查看电路信号,发现在ads1248芯片供电引脚AVDD以及自IEXC1恒流源出来经PT100和参比电阻相关电路,在温度测试异常时,均出现了下图所示纹波。

测试结果正常时,没有该纹波产生。并且,我们检测到,5V转3.3V稳压电路出来的3V3_A过磁珠FB1是有该纹波的,而另一块过磁珠FB2的3V3_D是没有该纹波的。
并且,将磁珠FB1短接或替换为0Ω电阻,该纹波消失,且温度测试结果也恢复正常。
且同时在研究ads1248数据手册时,发现其在第10.3节Do's and Don'ts (continued)中贴图(如下图),不允许2个电源和地信号之间接电感,但手册上并未说明原因,望有知晓的可以告知一下,万分感谢。

所以有着一些疑惑不解,由于板子存在用热风枪焊取过参比电阻R140,不知道会不会对芯片产生影响,测温结果异常偏差到底是由于ads1248本身的异常还是电路磁珠的设计引入的问题,
确实困惑不解,希望能能获得各位解惑,不胜感激!