This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using the iinternal reference of DAC, Vref=2.5025V when all channels don't output. If one channel output 2.4V, Vref will transfer to 2.5033V. When more channels output, Vref will be more and more high. If all channels output 5V, Vref is changed to 2.510V.Because Vref is changed, the output voltage of channel is changed,affecting the accuracy of production.
The ref pin of chip has 100nf(0603) and 1uf(0603) capacitors.
Tested DAC8568, no the problem.
DAC80508使用内部参考,通道不输出的时候内部参考Vref=2.5025V,通道1输出2.4V,Vref变为2.5033V,随着通道输出的增到,Vref持续增大,当8通道都输出5V的时候,Vref变大到2.510V,由于Vref变化,输出的电压值也发生变化,影响产品精度了。
DAC80508 REF脚上有100nf(0603)、1uF(0603)的电容.
测试DAC8568,没发现这个问题。
您好,
REF管脚仅连接了100nf(0603)、1uF(0603)的电容吗?是否还连接了其他负载?
VDD电压供电是否稳定?是否会随输出电压的增加而波动?建议用示波器测量下供电电压 VDD 和基准电压 VREF的示波器波形
您测试了几块板子是这种情况?可以多测试几块板子吗?
建议也确认下芯片的购货渠道,最终来源是否为TI?
你好,amy
1、除了这两个电容,没有其他负载
2、vdd是buck电源输出的,tps53603,输出会有30mv以下纹波,但是vref不是应该很稳定吗?vdd在供电范围内,vref就要稳定啊,这么重要的参考还受供电纹波影响这么大吗?
3、2块板子上4个芯片都有类似问题
4、最终来源肯定是ti的,肯定不是盗版的(估计也仿不出来),我们公司是ti的重点客户,芯片都是正规渠道购买
VDD是DAC80508的模拟供电电压管脚,一般建议选用线性电源来供电,避免开关电源高频开关频率的影响;
内部基准电压是有VDD产生的,VDD的纹波大,应该会影响到基准电压的精度;另外,供电电压的纹波大,也会影响到输出精度,评估参数是PSRR(电源抑制比):
PSRR分DC PSRR和AC PSRR,如下截图,可以看出随着供电电源纹波的频率的升高,AC PSRR急剧降低;
建议换稳定的线性电源给DAC80508供电,禁用板子上的开关电源,再次测试DAC80508的输出和基准电压的输出,看是怎样的?