This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP7002 处理 1080p@30 的问题

Other Parts Discussed in Thread: TVP7002

您好:
      我使用TVP7002作为TMS320DM368的视频输入AD,手册中写TVP7002支持1080p50和1080p60,但是我目前想处理的视频源是1080p30,请问TVP7002能处理1080p30吗?如果可以的话,寄存器应该怎么写?
      谢谢!
  • 您好:
          TVP7002手册中有如下说明:
          The internal sync separator provides support for field rates (VSYNC frequencies) at or above 40 Hz. Separated VSYNC or an external sync separator must be used to support formats having field rates less than 40 Hz.
           我现在想用TVP7002采集1080p@30fps的YPbPr高清分量视频信号,是不是应该使用外置的视频同步分离芯片?
           麻烦您帮我推荐一款YPbPr高清分量视频的同步信号分离芯片。谢谢!