Other Parts Discussed in Thread: DAC5686, TRF3705, DAC3482, LMK04906, LMK03000
我用DAC5686 外部时钟模式,电路连接采用手册推荐电路 Figure48 Driving the DAC5686 With a Single-Ended TTL/CMOS Clock Source 右边的图,时钟信号由FPGA引脚输出,电平标准3.3VLVCOMS,对时钟的配置按照手册26页外部时钟部分推荐,当从FPGA提供的时钟小于120MHz,DAC工作正常。当提供的时钟超过120MHz,DAC无法正常工作,PLLLOCK引脚无输出,改变SEL[1:0]值仍无效,不知道什么原因,求指导
还有一个问题,DAC5686 提供了Full_bypass 功能,可以屏蔽掉所有内插滤波器,当我使用该功能时,即将config_lsb 寄存器的Full_bypass 位置1,DAC无法正常工作,所以必须使用内插滤波器,不知道该功能是怎么回事。