This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS12963EVM使用出现问题!

Other Parts Discussed in Thread: ADS1293EVM, ADS1293

您好,刚从TI买的ads1293EVM,使用中按照user guide说的,插上USB供电,只要从TI下载的ADS1293软件,装了msp430-ads的驱动,都是按照用户手册上说的做的,为什么出现不了三导联的图呢???是不是TI的测试板里面没有程序的原因啊,而且没有提供JTAG下载器,只要一个USB。求上手。O(∩_∩)O谢谢

  • TI的EVM板里已经预装了程序。

    你这样,先用信号源给ADS1293一个信号,相信你能在GUI上看到波形。

    特别注意初调试ECG是非常难的,建议用标准的电极,并且连上右腿驱动调。我们用几根短线,连在接口处,用手指捏着都能采集到信号。

  • 您好,十分感激您的回复。这样,evm板已经预装了程序,正确装好驱动后,现在在ADS1293软件上选择3导联就自动分配好了3导联ads1293内部寄存器了。应该可以测量了。

    实际上,点击测试时,电极什么都没有加时,波形为正弦波,最大幅值·1.47mv,可是加了电极RL,LL,RA,LA,后,测试的3导联波形十分杂乱,明天我贴下图。幅值有时高达几百mv。。。。

    不过我们的电极线倒是很长,有1米吧。。。可是就算长,不加电极线的时候,怎么会出现幅值为1.47mv 的正弦波呢??IN1-IN2没加电极)应该为0啊。。

    软件用时,总会出错,显示写寄存器0x00出错!!!

    请您帮我分析一下好吗??明天贴图!

  • 您好,十分感激您的回复。这样,evm板已经预装了程序,正确装好驱动后,现在在ADS1293软件上选择3导联就自动分配好了3导联ads1293内部寄存器了。应该可以测量了。

    实际上,点击测试时,电极什么都没有加时,波形为正弦波,最大幅值·1.47mv,可是加了电极RL,LL,RA,LA,后,测试的3导联波形十分杂乱,明天我贴下图。幅值有时高达几百mv。。。。

    不过我们的电极线倒是很长,有1米吧。。。可是就算长,不加电极线的时候,怎么会出现幅值为1.47mv 的正弦波呢??IN1-IN2没加电极)应该为0啊。。

    软件用时,总会出错,显示写寄存器0x00出错!!!

    请您帮我分析一下好吗??明天贴图!

  • 您好,EVM上是9孔的插孔,那我们用的电极是不是也得是9针的?目前市场上貌似还没有这种电极!

  • 没错,市场大多都是15针的。。您也用过这个评估板?用起来了吗??我们可以交流一下。。我现在使用中,下面的报警灯都是red,除了BATlow。。

  • 你好,我想问一下你之前调的ads1293最后效果怎么样?