This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

想利用DAC接到CPU上来控制DC/DC的输出,如何做?请大侠指点



第一种方案:输入12V,输出0V~9V,输出电流2A。

第二种方案:输入24V,输出0V~12V,输出电流2A。

需要说明的是,用软件控制输出电压的多少。

需要DAC来控制DC/DC的输出,请问有没有电路可参考的?

谢谢