This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两片ADC08D1520同步问题

Other Parts Discussed in Thread: ADC08D1520, ADC07D1520

你好,

我们想用两片ADC08D1520实现对同一信号进行同步采样;

实验场景为:用同一时钟给两个芯片的CLK提供时钟;

实验结果是:两片ADC08D1520的DCLK每次都有相位差,而且相位差不固定。

是不是不能用两片ADC08D1520实现同步采样?或者有什么办法实现两片ADC同步采样?

谢谢!

  •  这颗芯片对华禁运,需要许可证(License)才可在华使用。请确认你已与TI签过license,否则TI不提供任何技术支持。

  • 两片ADC07D1520同步问题

        我正在使用TI公司的两片ADC07D1520芯片对同一信号进行同步采样,现遇到类似问题,还麻烦帮忙解决一下!

          
           场景:由同一时钟源给两片ADC07D1520芯片提供采样时钟,采样频率相同;两片芯片都设置为(Dual-Edge Sampling)DES模式和 1:2 Demultiplexed Mode;待采样的信号源为单载波;
           问题1:两片芯片的采样结果存在相位差;并且在单载波频率固定,采样频率固定的情况下,断电重新下载程序后(程序一样),每次采到的两个信号相位差不同(大于2个);
                       这样的话,是不是不能用两片ADC08D1520实现同步采样?或者采用什么办法可以实现同步?并且FPGA依靠什么确定两块芯片已经同步了?
           问题2:我有看到可以借助DCLK_RST信号来确定DCLK和CLK之间的相位关系,但DCLK_RST信号的下降沿必须与采样时钟CLK同步。
                       当采样时钟很高的时候(比如1.2GHz),FPGA不能接受这么高的时钟,DCLK_RST由FPGA产生,我如何保证DCLK_RST满足所需要的时序关系?
          麻烦尽快回复!很着急!谢谢!
  • 两片并行很难实现的

    不论做交织采样还是什么