This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293功耗和采样频率的问题?

Other Parts Discussed in Thread: ADS1293

1、ADS1293资料上写每个ADC通道的功耗为0.3mW,但我启动ADC数据转换后(即set address 0x00=0x01),ADS1293会增加近60mA的整机电流,而且我已经把所有的寄存器都已经设置到最低功耗模式,但只要启动ADC数据转换就会增大60mA。请问在3V供电下,3通道所有功能全开时,ADS1293的最大功耗为多少?我现在遇到的这个故障应如何排查,外围电路或者I/0口要注意哪些?

2、ADS1293的数据采样频率资料上写可达到25.6KSPS,但我通过MCU定时器中断去采样时,发现达到6.4ms左右一次中断后,再加快中断的速度,也就是增加采样点时,不能采集到更多点,应该是ADS1293数据建立时间的问题,请问这里是我在什么地方有理解错误吗,在哪里有设置错误,该如何增加采样点?