我的原理图我发附件吧,之前发过一个帖子说只有2路波形,其他6路波形干扰很严重,后来用50HZ软件滤波才能清晰看到其他6路波形,但是总电流很大,我测了一下AVDD那一路电流挺小的,5mA以内,DVDD那一路28mA,还望TI员工给看看,谢谢~~!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的原理图我发附件吧,之前发过一个帖子说只有2路波形,其他6路波形干扰很严重,后来用50HZ软件滤波才能清晰看到其他6路波形,但是总电流很大,我测了一下AVDD那一路电流挺小的,5mA以内,DVDD那一路28mA,还望TI员工给看看,谢谢~~!
你的AVDD和AVSS是多少?AVDD-DVDD是多少?按手册第6页的指标,IDVDD最多也就是0.5mA,怀疑是哪里短路了。你先不要用AVSS供电了,就用外部的3.3V和0V做AVDD和AVSS,用外部的1.8V或者3.0V做DVDD。所有的引脚,都按照0V做参考,看看效果如何。
1. 你的电路图上有一颗外部晶振HC735-2.048MHZ,这颗芯片使用DVDD供电的,塔的功耗是多少?如果有这颗芯片的手册,可以查一下。
2. 查阅手册,把数字域里能够power down的部分全都power down,看看哪部分关断之后,电流有明显下降。
3. 是否从正规代理商购买?