Other Parts Discussed in Thread: ADS1146
读了数据手册后,有如下的困惑:(以ADS1146为例)
1、可以通过产生一个START的脉冲来启动一次AD转换,或者将START持续拉高进行连续的AD转换,这两种操作方式和通过SPI写入控制命令RDATA和RDATAC有何区别?两者是否是独立的?通过SPI写控制命令的时候,是不是就和START的高低无关了?
2.、ADS1146的外接时钟,以4.096MHZ为例,这个时钟频率是用来决定采样频率的么?那数据的传输速率又由谁决定呢?比如2kSPS和5SPS的传输速率下,对SCLK的速率是否有要求?
3、如果通过START脉冲或者RDATA单次转换的方式控制ADC,上述数据传输速率是否还有意义?
谢谢!