1、对ADS1018的内部PGA进行设置,分别使用2/3、1、2、4、8、16倍放大,但是通过数据转换后,在这6种放大倍数下,实际信号放大倍数为1/3、0.5、1、2、4、8,如采集238.0mV的信号,PGA设置为2/3、1、2、4、8、16倍,输出数据分别为79、119、239、478、956、1911,配置值分别为0xC1CB,0xC3CB,0xC5CB、0xC7CB、0xC9CB、0xCBCB,读取数值都是在设置重新设置好后,第三次的数据读取值。
2、在32位数据模式下分别采用连续发送两次配置命令和第一次发送配置命令 第二次发送0x00,读取配置命令返回值,前一种情况返回值都是错误的,第二种情况可以正确读取。
3、在设置PGA后很多时候需要重新给ADS1018重新上电才能执行新的配置,这是必须操作吗?