This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
void ADS8345_start(void)
{
DCLK = 0;
CS = 1;
DIN1 = 1;
// DOUT = 0;
DCLK =1 ;
CS = 0;
// BUSY = 0;
}
void ADS8345_WR(uchar dat)
{
uchar count;
DCLK = 0;
for(count = 0; count < 8; count++)
{
dat <<= 1;
DIN1 = CY;
DCLK = 0;
_nop_();
_nop_();
_nop_();
DCLK = 1;
_nop_();
_nop_();
_nop_();
}
}
uint ADS8345_RD(void)
{
uchar count = 0;
uint dat = 0;
for(count = 0; count < 17; count++)
{
dat <<= 1;
DCLK = 1;
_nop_();
_nop_();
_nop_();
DCLK = 0;
_nop_();
_nop_();
_nop_();
if(DOUT == 1)
{
dat++;
}
}
return (dat);
}
void main()
{while(1)
{
ADS8345_start();
delay(2);
ADS8345_WR(0x87);
DIN1 = 0;
// delay(2);
DCLK = 0;
_nop_();
_nop_();
_nop_();
_nop_();
DCLK = 1;
_nop_();
_nop_();
_nop_();
_nop_();
//while(BUSY == 1);
result = ADS8345_RD();
CS = 1;
AD_result = (double)result * 5 / 65535;
}
}
模拟部分,检查各个输入的绝对电压是不是在(-0.2,VCC+0.2)这个范围。检查VREF是不是在(0.5,2.5)这个范围。
数字部分,可以参考图8或图9来检查波形是不是和手册一致。
AD_result = (double)result * 5 / 65535;
为什么是*5?手册15页左边那个表格,是数字编码和输入信号的关系,你检查一下你的程序和这个表格是不是吻合的。
怎么可能算出来56458和65534?!按手册15页的data format,输出应该在-32768~32767之间啊。你是不是把2的补码搞成二进制偏移码了?
不能这样理解。如果是二进制偏移码(offset binary),那么编码范围是0~65535,都是正数。如果是二进制补码(2's complementary),那么编码范围是-32768~+32767,有正有负,但是一样是65536个数,只不过中点从原来的32768移到了0,不能因此就说这是个15位的。如果想把补码转成偏移码,可以在处理器里做个简单运算即可。至于偏移码和补码的具体表示方法和区别,你可以查一下相关资料,网上应该有很多。
如果是单端输入VREF=2.5V,在单5V供电下,由手册第10页analog input单端输入所示,编码值应该在0x0000附近。请提供你的编码值是多少,以及4.98V是怎么算出来的。
哦 但是阅读PDF是这一段疏忽了 我大概的看了一下 理解如下 您看一下我是不是可以这样理解呢 就是说我单端输入的话, 基准电压在2.5v的时候AD采集会的数据只能是在2.1v~2.8v之间么 要是基准电压是0.1v的时候 AD可以采集回来的值是0.1v~4.9v么?(谢谢您之前的回复)
为什么是2.1~2.8??手册第10页,analog input上说得很明确了,单端输入,如果单端的共模点和VREF相同,则把COM接到VREF,电路的输入范围可以达到2*VREF。举个例子,输入是0~5V,单端,共模点是2.5V,等于VREF,则此时把COM脚连到VREF上,输入可以支持的电压范围就是(VREF-VREF,VREF+VREF),即(0,5)。如果共模点不是2.5,而是2,则设法把2V的共模提取出来,连接到COM,ADC的输入可以支持的电压范围就是(-0.2,4.5),-0.2是ADC可以接受的最低电压。