This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS1206的data_av信号问题

Other Parts Discussed in Thread: THS1206, LM324

您好,我在使用THS1206,AVDD=5V,BVDD=DVDD=3.3V;

输入时钟为3MHZ,和FPGA进行连接;

测试data_av信号输出的高电平和低电平都是mv级别的,请问是什么情况呢?

  • 你好!

    Data_AV 是数字输出脚,建议你把后面的负载先断开,看看是否是负载太重的缘故,我看规格书中的描述,其测试条件是IOH=-50uA. 即其负载最还大于100Kohms.

  • 感谢您的回复,按照您的指导,我测试了一下,发现Data_AV确实高电平为3.3V,低电平为10mv左右。

    那么问题就是如您所说,那我该如何处理呢?

    另外,我之前只焊接了THS1206,在测试模式下测试正确,后来焊接了LM324对模拟输入电压范围进行了平移改变,LM324的同相输入端使用的THS1206的参考输出电压2.5V,然后测试模式下就不对了,切断二者之间2.5V的连接,使用独立电源作为LM324的同相输入,也不对,是不是因为THS1206芯片烧了?

  • 感谢您的回复,按照您的指导,我测试了一下,发现Data_AV确实高电平为3.3V,低电平为10mv左右。

    那么问题就是如您所说,那我该如何处理呢?

    另外,我之前只焊接了THS1206,在测试模式下测试正确,后来焊接了LM324对模拟输入电压范围进行了平移改变,LM324的同相输入端使用的THS1206的参考输出电压2.5V,然后测试模式下就不对了,切断二者之间2.5V的连接,使用独立电源作为LM324的同相输入,也不对,是不是因为THS1206芯片烧了?