请教:我在用ADS1232接称重传感器时,在稳定性测试中遇到一个现象,称重传感器空载,在上电复位后,读取ADS1232的输出AD值,该值会一直慢慢的持续递减,比如刚开始读取的是77700,过个20分钟,会变成77600,再过20分钟会变成77500,就这样一直持续递减下去,有人问我会不会递减到0,我说不知道,因为没办法测试那么久时间,搞的我很郁闷,请各位指教!由衷的感谢!
附件是AD输出曲线图和原理图(AD参考电压2.5V),请各位帮忙。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教:我在用ADS1232接称重传感器时,在稳定性测试中遇到一个现象,称重传感器空载,在上电复位后,读取ADS1232的输出AD值,该值会一直慢慢的持续递减,比如刚开始读取的是77700,过个20分钟,会变成77600,再过20分钟会变成77500,就这样一直持续递减下去,有人问我会不会递减到0,我说不知道,因为没办法测试那么久时间,搞的我很郁闷,请各位指教!由衷的感谢!
附件是AD输出曲线图和原理图(AD参考电压2.5V),请各位帮忙。
顶一下!实在不好意思,有时候有的问题不能很快就能提出解决方案,我们尽快给您回复。谢谢您理解!
你好,
看到你的测试和电路,有几个建议希望对你有用:
1.在数据变化的时候,是否有测试模拟输入端?这个输入是变化的?
2. 将你原理图中的C15/C18去掉,进行测试。
目前正式渠道还是通过上网进行申请样片或评估板,不知道您是否试着通过代理申请?对于ADS1232REF评估板,我这边也帮您问一下。。。