Other Parts Discussed in Thread: DAC5687, DAC5686
我购买了德州的dac3162和其评估版,根据软件存入的数据表都是正的信号,存入一个阶梯波的excel数据,但最终输出的波形出来的却是正负电压的波形,波形正确,但电压不对,请问为何以及如何解决呢?



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您是使用的变压器耦合输出吗?变压器输出是AC耦合输出,它输出的信号没有直流成分,如果要想只有正值输出,需要使用DC耦合输出,下面帖子中的附件信息希望对您有帮助:
不可以的,需要考虑其直流偏置和AC耦合输出阻抗;您可以使用R203和R211及后端电路配置成如下接图:

注意需去掉R109、R110,因为变压器4脚至6脚电感对于直流偏置是相当于短路的。
具体您可以查看下面文档的3.1章节:
Passive Interface for Current Output DACs
文中提到的Excel计算表格:
DAC3162模拟输出合规范围是AVDD-0.5V至AVDD+0.5V,因此它的DC耦合输出需要考虑其直流偏置;
因为DAC3162是高速DAC,既然使用它那么其工作信号频率应该比较高,因此需考虑交流阻抗匹配;
上图输出单端配置中DAC5686 DAC5687是与DAC3162有一样的输出合规电压,因此可参考这个电阻网络,在电阻器网络之后可加运放电路以驱动后级负载。