This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: AD1293芯片在进行YY0885测试的时候输入阻抗影响了波形

Part Number: ADS1293


我们使用了AD1293芯片,在进行YY0885测试的时候,加入了620KΩ的输入阻抗后,10Hz的正弦波形只画出来三个周期就变成直线了,是什么原因导致的呢?

  • 您好,

    所附图片中记录器是指ADS1293吗?图中开关状态是怎样的?P1至P6是指ADS1293的6个模拟输入吗?300mV DC可调信号的参考点接在哪里?

    10Hz的正弦波形只画出来三个周期就变成直线了

    检查下是否为接线不牢固导致的问题?

  • Hi Amy,

    记录器是只ADS1293;波形有影响的时候,图中的S1开关是断开状态;P1-P6是心电模拟仪的输出点;300mv DC可调信号的参考点认为是接在了LA上。接线牢固的。

    Thanks & Best Regards

  • 坦白讲我不明白 YY0885测试,您可以尽可能详细描述吗?它测试的是什么?

    测试时心电模拟仪对P1-P6有输入吗?

    10Hz的正弦波是接入上图中最左边交流信号模型处吗?

    “10Hz的正弦波形只画出来三个周期就变成直线了”,这里的输出是指用 ADS1293采集的P1端输出的数字信号画出来吗?输入10Hz的正弦波时,P1端信号波形是怎样的?还是说ADS1293采集的是P1至P2间的差分信号?如果是P1至P2间的差分信号,那么这个差分信号波形实测是怎样的?