This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1306E05: 模拟输入电压超过AVDD,输入的限流电阻如何计算

Part Number: AMC1306E05


我使用AMC1306测量24V电源上的输出电流,AVDD供电用5V,datesheet中输入电压超过AVDD的范围,应该把输入电流限制在10mA以内,问一下,这个限流电阻怎么计算?

  • 您好,

    是的,可以串联限流电阻将输入电流限制在10mA以内,但是这是应用在过压(电压瞬变过压)保护的情况下,如果让设备长时间处于这种过压下可能会缩短设备的寿命。

    限流电阻的计算:输入24V,高于供电电压5V的电压是19V,串联1.9k电阻可以将电流限制为19V/1.9k=10mA。

    增加限流电阻器还需要注意一个问题,即设备的输入失调电流会在限流电阻上产生压降,形成输入失调电压。

  • 你好,

        那我测量24V的电流,先用隔离电源将24V转5V,再给AVDD电源供电,这样操作吗?

  • 我不确定您这里的问题是什么?

    如果AINP, AINN管脚的输入电压超过AVDD的下述范围:

    您可以使用低侧测量24V回路的电流,像datasheet figure 59 这样: