This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DL040: 芯片内部的VREF管脚

Part Number: ADC12DL040


在一个产品中VA、VD和VDR管脚是用3.3V供电的,VREF管脚刚开始是用1K电阻接到3.3V上,此时发现芯片会发烫,请问是何原因。后来断开1K电阻,Vref管脚处于悬空状态,此时几个板子算下来内部VREF电压都是1V,实际测量芯片的7脚会出现1.5/1.8/2V这些电压,各个单板不一致,请问是何原因。如果VREF管脚悬空的话,是否可以保证ADC用的是芯片内部的1.0V refrence。

  • 您好,

    芯片发烫时,实测供电电压是否稳定、是否在正常供电范围内?模拟输入电压是否在ADC规定范围内?各信号地是否共地?

    Vref 内部集成了上拉,应该是默认使用内部1V基准电压的;

    因为Vref 是输入管脚,不应作为输出管脚进行测量,实际测量芯片的7脚会出现1.5/1.8/2V这些电压,我想可能是因为它是输入管脚的原因,受外部测量电路的影响。

    关于VREF管脚使用1K电阻接到3.3V上发烫的现象,还是建议查明原因,以排除隐患。