This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81416: DAC81416:

Part Number: DAC81416


DAC81416没有输出。硬件是这样的:VIO为3.3V,vDD,VAA为5v,vcc为12v,vss接GND.TOGGLE0,TOGGLE1,TOGGLE2,LDAC,RESET,CLR 接STM32的IO,上电后RESET拉低10ms后拉高。TOGGLE0,TOGGLE1,TOGGLE2,LDAC,CLR均拉高。先REF接2.5V,测量REF为2.5v,测量REFCOMP为0v,感觉不对;改接REFCOMP 为2.5v,测量REFCOMP为2.5v,测量REF为1.7v左右。GENCONFIG=0X4000,SPICONFIG=0X0A84,DACRANGE0=0X1111,DACRANGE1=0X1111,DACRANGE2=0X1111,DACRANGE3=0X1111,DACPWDWN=0X0000.

  • 您好,REFCMP 是否有接330pF补偿电容到地?这个引脚建议接330pF到地。我看到GENCONFIG您配置的是内部参考disable,使用的外部参考。 我们可以先enable internal reference 进行debug。比如上电期间,器件进入power down状态,内部参考电压disable,当电压完全起来稳定之后,internal reference enable,此时测量下REF电压是否为2.5V,如果是1.7V 则是不正常的。如果测量2.5VREF,则说明SPI frame是没问题的,能正常写入。