This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL0102-100: i2c读写测试正常,阻值变化对不上。

Part Number: TPL0102-100


原理图如下:

1)8位I2C地址是0xA0,测试可以正常读写寄存器。下图时捕捉到的时序。、

2)测试时R22电阻断开,

      -->寄存器WRB和WRA都给0x00,测试HA引脚到地的阻值位52.4K

      -->寄存器WRB和WRA都给0xff,测试HA引脚到地的阻值位9.5K

      -->寄存器WRB 0x00和WRA给0xff,测试HA引脚到地的阻值位9.5K

      -->寄存器WRB 0x00和WRA给0xff,测试HA引脚到地的阻值位9.5K

  • 您好,

    上面时序是对应的以下操作吗?

    写寄存器地址0x00,写入值为0x00;

    写寄存器地址0x01,写入值为0x00;

    读寄存器地址0x10,读出的值为0x40;这一步可以验证寄存器可以正确读出来,因为寄存器默认值是0x40;但是并没有验证寄存器可以正确写入,验证寄存器可以正常写的过程是对一个寄存器地址写入一个值后可以正确读出来。您对上述寄存器写入后,是否通过读出来以验证可以正确写入?

    TPL0102集成的两路电位计在功能上是相互独立的,您可以分开单独测量它们的输出吗?