Other Parts Discussed in Thread: OPA277, THS4051, OPA727, OPA704
DAC8831在未接后级负载(功率放大模块)时,输出一切正常,但是接入功率放大模块时,用万用表测量功率放大模块输出后,DAC8831输出的电压变成负值,严重偏见设定的正值,用开发板的DAC未出现这种情况,这是DAC芯片出现了问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,DAC8831是unbuffered DAC,带载能力很弱,后端需要接buffer;
TL072I带负载能力也不强,因此建议您使用DAC8831数据表中推荐的运放;
另外能否推荐几款与DAC8831性能参数相近的DAC芯片
您这里是指哪方面的性能?或者您需要推荐DAC是基于哪方面因素的考虑?知道了这些才能更准确的向您推荐DAC
TL072I带负载能力不强,不建议使用,建议使用DAC8831数据表中推荐的运放,比如OPA277、OPA704、OPA727。
STM32上的DAC可以,这个带负载能力更强吗?
STM32上的DAC是buffered DAC吗?buffered DAC驱动能力强一些;
单通道,抗干扰能力强,带负载能力强,±2.5v输出
对Resolution、Settling time、update rate (MSPS)有要求吗?
我初步筛选了以下型号: