This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8831: DAC8831受后级放大电路影响

Part Number: DAC8831
Other Parts Discussed in Thread: OPA277, THS4051, OPA727, OPA704

DAC8831在未接后级负载(功率放大模块)时,输出一切正常,但是接入功率放大模块时,用万用表测量功率放大模块输出后,DAC8831输出的电压变成负值,严重偏见设定的正值,用开发板的DAC未出现这种情况,这是DAC芯片出现了问题吗?

  • 您好,

    您测试了几块电路板是这种情况?用万用表测量功率放大模块输出不应影响DAC的输出,检查下测试时是否接线错误?

    测试电路板电路与EVM板是一致的吗?如果电路是一致的,那么排除接线问题后,可能是DAC芯片的问题,需要确认DAC购货来源。

  • 就买了一块,我是用DAC8831+TL072I替换了手册的DAC+OPA277,输出的-REF-0-+REF,进行放大4.4倍(68k和20k组合)后的电压作为功率放大模块的输入(接THS4051),如果用ARM开发版的DAC输出作为功率放大模块输入。万用表测量不受影响。是否是因为DAC8831带负载能力弱,输出的-REF-0-+REF,需要再接一个电压跟随器再放大4.4倍。另外能否推荐几款与DAC8831性能参数相近的DAC芯片

  • 就买了一块,我是用DAC8831+TL072I替换了手册的DAC+OPA277,输出的-REF-0-+REF,进行放大4.4倍(68k和20k组合)后的电压作为功率放大模块的输入(接THS4051),如果用ARM开发版的DAC输出作为功率放大模块输入。万用表测量不受影响。是否是因为DAC8831带负载能力弱,输出的-REF-0-+REF,需要再接一个电压跟随器再放大4.4倍。另外能否推荐几款与DAC8831性能参数相近的DAC芯片

  • 是的,DAC8831是unbuffered DAC,带载能力很弱,后端需要接buffer;

    TL072I带负载能力也不强,因此建议您使用DAC8831数据表中推荐的运放;

    另外能否推荐几款与DAC8831性能参数相近的DAC芯片

    您这里是指哪方面的性能?或者您需要推荐DAC是基于哪方面因素的考虑?知道了这些才能更准确的向您推荐DAC

  • 添加了一个TL072I的电压跟随器也不行。STM32上的DAC可以,这个带负载能力更强吗?单通道,抗干扰能力强,带负载能力强,±2.5v输出

  • TL072I带负载能力不强,不建议使用,建议使用DAC8831数据表中推荐的运放,比如OPA277、OPA704、OPA727。

    STM32上的DAC可以,这个带负载能力更强吗?

    STM32上的DAC是buffered DAC吗?buffered DAC驱动能力强一些;

    单通道,抗干扰能力强,带负载能力强,±2.5v输出

     

    对Resolution、Settling time、update rate (MSPS)有要求吗?

    我初步筛选了以下型号: