This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8718: DAC8718不同供电,最小输出电压怎么判断?

Part Number: DAC8718

我想请教一下,DAC8718(7718)在单电源供电,双电源供电,两种方式下,输出的模拟电压最小能到多少?

我看规格书上:

Note that the maximum output voltage must not be greater than (AVDD – 0.5V) and the minimum output voltage

must not be less than (AVSS + 0.5V); otherwise, the output may be saturated.

是否可以这样理解:

如果单电源供电,最小电压应该只能到0.5V

如果双电源供电呢,比如正负15V,最小输出电压能到-14.5V吗?

我的设计上想用到最小0.3V的电压,如果这个DAC能用,那我用哪种方式供电,才能满足要求?

谢谢解答回复!

  • 您好,

    DAC8718在双电源供电时,输出范围是双极性的,因此包括0V,最小是AVSS+0.5V,最大是AVDD-0.5V;

    在单电源供电时,输出范围是单极性的,最大是AVDD-0.5V,最小受限于输出运放的电压摆幅,根据datasheet描述最小是负供电电压以上0.5V,单电源供电时就是0.5V,但是看Figure 85,如果sink电流比较小,应该可以满足您最小0.3V的电压要求,这个主要看您应用的sink电流的大小。

    总的来说双电源供电最小可以到0.3V。