This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1118EVM: 输入电压和输出值问题

Part Number: ADS1118EVM


您好,

   我在你们官网购买ADS1118EVM 的demo板,买回来以后,我进行了测试,测试图片如下:

1.按照你们的EVM手册进行连接,在AIN0 和GND 接了1V 的电压,通过下面的板子usb连到笔记本,通过GUI软件查看数据,发现出来的数据只有0.几V,并不是1V,所以我不太理解出来的数据为什么不对呢?可以查看第二张截图,是我配置的不对还是什么原因呢?

我Y 轴显示的是volts不是codes

2. 还有一个问题就是Y 轴显示那个codes是什么意思?我怎么对应输入进来的电压值呢?

  • 您好,

    Config Register配置的是什么?默认下是差分输入AIN0是正输入端,AIN1是负输入端:

    codes是输出代码,输出代码乘以1LSB就是对应的输入模拟电压,LSB大小由PGA配置选择: