Other Parts Discussed in Thread: ADS1298,
我设计了一块采集心电的板子,电源通信都留出了接口,dvdd接3.3V mcu(spi 3.3V的mcu)可以正常通信,但是改为1.8V(spi 1.8v 的mcu)给dvdd供电后 使用逻辑分析仪查看 可以看到MOSI正确的发送了数据,但是MISO一直返回0,请问这是什么情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
3.3V跟内存卡共用
内存卡是否支持1.8V供电?3.3V换1.8V后,内存卡是否还能正常工作?内存卡是否影响ADS1298的正常工作?
数字地和模拟地需要共地,但是也请确认下ADS1298是否与所使用MCU共地?
ADS1298的AVDD、AVSS是采用3.1V单电源供电是吗?AVDD-AVSS=3.1V也没问题;
总之,ADS1298的DVDD可以使用3.3V或1.8V供电,这是没问题的。因此建议检查接线是否有误、接线是否牢固和实际供电电压是否符合期望值。