Other Parts Discussed in Thread: DAC11001B
Hi there,
I use BP-DAC11001EVM to test the output voltage of dac11001b.the output voltage is about 2.5V, VREFP =5V, VREN=-5V, I tested the output voltage ten times, and the maximum value minus the minimum value is equal to 15uv. However, I found in figure 6-42 of datasheet that the DAC output noise is only about 0.4uv. What methods can be used to improve the stability of the output voltage? thank you