This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1291: ADS1291的采样率不准问题

Part Number: ADS1291


1.使用ADS1291内部时钟时,设置采样率为1k,测的DRDY引脚频率是1kHz,1.002kHz,1.004kHz,1.006kHz。为什么不是稳定的1khz?

2.且有的drdy引脚的低电平宽度比其他的宽。请问这是什么原因呢?

3.如果使用外部时钟,频率必须使用2.048Mhz或者512khz吗?是否可以使用其他频率?

  • 您好,

    1、内部时钟并不是稳定在一个值,它有个精度范围:

    另外,与供电电压的干净度也有关:

    2、DRDY在随后的第一个SCLK下降沿变高,我想您应该对比SCLK信号一起看,看是否因SCLK上升沿的位置不同导致的DRDY宽度不一致;

    3、不是的,可以使用其他频率,在最小值和最大值之间的值都可以。

  •  这里只有2个选择,能设置成其他频率。我设置成2M,采样率也是不准。1k只有978hz。

    不是的,可以使用其他频率,在最小值和最大值之间的值都可以。
  • 3.如果使用外部时钟,频率必须使用2.048Mhz或者512khz吗?是否可以使用其他频率?

    我上面的回复是针对的您的第3问,即外部时钟输入频率范围:

    我设置成2M,采样率也是不准。1k只有978hz。

    使用外部时钟,那么外部时钟也有个频偏范围,同时也与供电电压的稳定性和噪声性能有关;