This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: 两个ADC同步采样的可能性

Part Number: ADS1263


Hello, my application needs to sample two channels synchronously, but the current resolution of synchronous sampling ADC is 24 bits, and the noise level is not ideal. Is there any way to achieve synchronous sampling of 2 ads1263? Hope the synchronization is within 5 microseconds, thank you!

  • 您好,

    但目前的同步采样adc分辨率是24位,噪声水平也不理想,

    ADC涉及的噪声源比较多,每一处都需要注意以避免引入噪声。噪声源包括各被采集信号的纹波或噪声、供电电压、基准电压、时钟信号、Layout等引入的噪声。

    被采集信号是否为干净稳定的信号?首先需要排除这个原因;

    供电电压一般建议采用线性供电电源。开关电源带有高频开关信号,处理不好会影响ADC的精度。

    基准电压如果使用内部基准也建议检查其稳定性及纹波;

    时钟信号是否干净或jitter大小;

    有什么方式可以实现2个ads1263的同步采样吗?希望同步达到5微秒以内

    ADS1263采样时钟源是CLKIN,同步达到5us以内,两个ADC的同步程度与CLKIN的频偏和jitter有很大关系,另外就是考虑怎样同步启动这两个ADC的转换,启动信号从主控端到达ADC的延迟要一样。我建议您考虑采用可以同步采样的多通道ADC以简化设计。

  • 感谢您的回复!关于双ads1263的同步采样,在《基于热敏电阻器的双AD高精度温度采集系统设计》这篇期刊中有实现,但没公布具体方法和同步情况,很期望TI开发相关的参考设计;关于您说的同步采样AD,我也在尝试,感谢您的建议!