This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278: 在不同采样频率下的非线性问题

Part Number: ADS1278

TI工程师您好:

  • 我们使用 ina 2128芯片放大来自压力传感器的24路信号,随后将信号输入ads 1278芯片,得到数字信号。
  • 实验测试ads 1278芯片的温度特性,其他实验条件相同,输入恒定信号,分别测试ads 1278在采样频率为512 fps和50 fps时芯片随温度变化的输出,输出信号如下图1,图2所示。可以发现,采样频率降低之后,输出信号的非线性得到明显改善。
  • 请问这种现象是ads 1278自身的特性引起的吗?有没有办法实现在512 fps的采样频率下仍能保持较好的线性?

期望您的回答