This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82EVM: 配置问题

Part Number: DAC38RF82EVM
Other Parts Discussed in Thread: TSW14J57EVM,

有新的问题请教您

1,配置DAC GUI的时候,在“Quick Start”tab,请问“# of IQ pairs per DAC”中选择一对、两对和“real input”的含义。

2,请问“# of serdes lanes per DAC”的含义。

3,请问“DAC Clock Frequency(MHz)” 和“Sampling rate”有什么关系。

4,请问DAC38RF82EVM上的指示灯D8“JESD SYNC”不亮,该如何解决,是否代表DAC38RF82EVM与TSW14J57EVM未同步成功?

5,按照步骤点击“Reset DAC JESD Core & SYSREF TRIGGER”时,TSW14J57EVM上的指示灯D1灭了一下又亮了,是否代表DAC EVM与TSW EVM没有成功建立同步连接?

6,DAC38RF82EVM给它输入5v的直流电压,但是测它的正负脚电压为4V,请问这个压降正常吗?在还没配置这块板子的时候电流大概是1.6A,配置之后有时候还有2点多安培。另一块板子TSW14J57EVM电压测试就是12V,没有问题。