This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求教:
我的应用场景是这样的:
有一个电流输出回路,我在电流输出回路中串入一个20欧姆的采样电阻,将采样电阻两端的电压经过AD8223之后,转换成单端输入到ADS1259的输入端。ADS上电后配置成连续转换模式。参考电压2.5V,内部参考电压模式。1秒钟输出60个数,没有start引脚,通过命令启动。
问题:如果输入端是一个相对稳定的电压,即上下变化上百mV,ADS1259的输出结果一直很正常。但是如果以1秒钟1%的增量增加时,当增加到92%左右,ADS1259就会输出一个饱和值,这个时候reset单片机没有任何效果,只有重新掉电再上电,ADS1259的输出结果又恢复正常。
反复试验,很容易复现这个现象。
实在是想不明白,求大神指教
您好,
您可以附上采样电阻+AD8223+ADS1259电路图吗?
“当增加到92%左右”是指电压是多少?
"ADS1259就会输出一个饱和值"是指输出code是7FFFFFh吗?
“ADS1259的输出结果又恢复正常。”这里是指输出结果可以转换为正确的对应的输入电压吗?,即增加到92%左右的输入电压?