在ADS1115和做缓冲的运放之间加了个RC滤波,但是R的两端产生了0.2V左右的压差,我这儿选择的R为51欧姆,电容C为22uF,有谁知道电阻和电容的合适取值,而不至于影响采样精度?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对照手册第10页通道连接图,查一下是不是有什么泄露的路径。另外,最好能上传一下电路图以便分析。
如果0.2V是用万用表量的,那么怀疑有泄露路径,泄露路径可能是AIN0-->AINx (x=1,2),这个可以参考手册第10页图22。你可以试试把AIN1和AIN2前级的运放/电阻断开,使AIN1和AIN2往外看,看到的是一个高阻,然后再测AIN0通路上R两端是否有压差。如果没有了,那泄露路径可能就是AIN1或AIN2。
手册第三页倒是有提到Common mode input range,适合PGA Gain有关的,你的PGA Gain是多少?看上去,有些情况下输入端不能短接到地,可以试试输入端接到AVDD/2这个电平,再看看会不会有偏差。
同时,可以试试把50欧姆的滤波电阻改成100欧姆,200欧姆。。。看看降落在电阻上的电压会不会增大,如果有增大,那么确实有泄露通路,就需要再去检查到底电流是从哪里泄露出去的。