Part Number: ADS1291
你好,是这样的,我想咨询RLD寄存器问题,当我想采集外界信号时,如果按照之前工程师你说的设置:将RLD设置为00,不让RLD与通道1正负极连接,出来的数据断断续续,还不是外界信号。如果让RLD与通道1正负极连接,并且启用RLD缓冲器和RLD感应器,可以采集到数据显示波形 ,但是导联脱落检测不到RLD线脱落情况,这个该怎么解决?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
https://e2echina.ti.com/support/data-converters/f/data-converters-forum/290608/ads1291
在这个帖子里我这里建议将RLD禁用,是希望将 ADS1291设置成普通的ADC来采集信号,以验证其可以正确AD转换和code转换;如果您外界输入的是模拟ECG信号发生器,需要RLD反馈电路的话,那么禁用RLD后AD转换输出肯定是不正常的。
看您这个帖子问题说明,是不是ADS1291已经可以正确AD转换和code转换了?
关于RLD脱落检测问题,需要说明的是:只有在RLD放大器power down时,RLD导联脱落感应功能才有用。否则,RLD输出将始终被驱动到中电压,比较器将永远不会检测到RLD电极的导联脱落事件。