This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC122S051: 关于adc122s051采集精度受电源精度的影响

Part Number: ADC122S051


请问adc122s051这类ad转换ic内部是否自带基准电源。芯片手册中提到Full Scale Error在常温下为1.5LSB,假如供电为5V,误差约为1.8mV。若芯片电源精度较差,实际供电为4.9~5.1V。

那么实际最大误差是否就是0.1V,约82LSB呢?

  • 您好,

    ADC122S051 内部没有集成基准电压,基准电压是使用的供电电压VA

    Full Scale Error 可视为传统的规格参数增益误差Gain Error,如下截图所示:

    那么基准电压的变化对输出的影响应该是:

    1LSB=5V/4096,若基准电压5V变化ΔV=±0.1V,那么ΔLSB=±0.1V/4096,在满量程输出时误差最大,即±0.1V。

    因此,是的,是您计算的0.1V,约82LSB