Part Number: ADS125H02
图纸参考了参考设计,原理图如下图

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是不是与前端输入信号的接线有关,您可以给出直接输入端接到实验室电源的接线图吗?输入信号是否与 ADS125H02 共地?
异常时的输入信号幅值是多少?AD芯片的供电电压和基准电压是多少?gain设置多少?我想看下输入信号是否满足ADS125H02 的输入信号范围
被测信号要和ADC共地的,ADS125H02有共模和差模输入电压范围要求,不共地对ADC来说就没法定义输入信号范围,那么其输入电压就是不确定的。
另外请注意,上图中仪器电源和220VAC转12VDC电源适配器都是变压器隔离电源吗?如果都是或都不是的话,直接共地没问题;如果不一致,即一个是隔离电源一个是非隔离电源,那么相关信号包括地信号不能直接相连。
还有一个新问题,其中的有一块板子,采样值不准,查了STATUS1寄存器,发现值为0xA0A0,PGA_L报警。外部电源啥的都正常,这有可能是什么原因呢?
ADS125H02 寄存器都是8bits的,您这里指STATUS1寄存器值为0xA0是吗?
您好可以用示波器测量输入信号吗?查看输入端是否存在瞬间幅值过大情况 因为PGA监视器是模拟比较器,可对瞬态过载情况作出响应。