This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292RECG-FE: 已安装ADS1x92xEVM-SW-installer程序但计算机设备管理器提示无法找到设备驱动,代码28

Part Number: ADS1292RECG-FE

1.操作系统为WINDOW7 64bit,

2.已安装VC ++2008和官网提供的安装程序

3.可以使用固件更新程序找到设备并更新.txt后缀的固件成功更新固件

4.使用USB接口从计算机主板后USB3.0接口连接,评估版D2 LED绿灯闪烁

问题:无法找到设备驱动,目前不确定是开发环境问题还是评估板本身问题,亦或其他原因导致,请求协助