This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299-4: 信号抓取

Part Number: ADS1299-4


您好,根据Figure67 上电初始化流程 ,我有一些疑问。比如我现在想要抓取内部测试信号,当我配置Con3为E0h完毕后,直接配置Con2为D0h,Con1为96h通道为05h,然后拉高start 发送RDATAC。或者  完全根据手册先配置Con3为E0h,Con1为96h,Con2为C0h,然后拉高Start发送RDATAC,随后发送SDATAC配置Con2和通道,然后捕获测试信号。    这两种做法有何区别